4/30/2016 7:38 PM | |
Joined: 3/28/2010 Last visit: 5/29/2024 Posts: 1032 Rating: (211) |
The LUT400 manual says (on page 79 pdf, Initial Device Setup) that the initial/factory setting for the 4-20mA output is set to 1.6mA. Don't ask me why . . . Link to pg 69 pdf Initial device setup Try reconfiguring the Low Calibration Point/LRV |
This contribution was helpful to1 thankful Users |
4/30/2016 8:46 PM | |
Posts: 15 Rating: (0) |
thank you :)... i will try and i will post what happened |
4/30/2016 8:49 PM | |
Posts: 15 Rating: (0) |
i've checked the link, it specifies the distance for low calibration ( 1.6 distance unit ) which will be assigned to 4 mA |
Follow us on