5/11/2016 8:49 PM | |
Joined: 12/18/2014 Last visit: 9/13/2024 Posts: 33757 Rating: (4191)
|
I mean like this. |
5/11/2016 9:06 PM | |
Posts: 200 Rating: (6) |
i have this set the same i just cant seem to connect what so ever one to download the program or to the logo AttachmentDoc3.pdf (259 Downloads) |
Last edited by: Min_Moderator at: 5/12/2016 9:06:11 AMConvert attachment to pdf |
|
5/11/2016 9:14 PM | |
Joined: 12/18/2014 Last visit: 9/13/2024 Posts: 33757 Rating: (4191)
|
If the Connection goes through a router? If so, what IP address has the router? |
5/11/2016 9:19 PM | |
Posts: 200 Rating: (6) |
my connection is as follows hmi to pc to down load the program to logo to pc to down load the program then hmi to logo |
Follow us on