(0)| 2/15/2006 4:34 PM | |
|
Posts: 1 Rating:
|
Hey I am working at a project but i am out of DO. I need at least 3 more DO. (35 in total) I am using now SIMATIC S7-300, DIGITAL OUTPUT SM 322, OPTICALLY ISOLATED, 32 DO, 24V DC, 0.5A, 40 PIN, SUM OF OUTPUT CURRENTS 4A/GROUP (16A/MODULE) 6ES7322-1BL00-0AA0 I found this one: SIMATIC S7-300, DIGITAL OUTPUT SM 322, OPTICALLY ISOLATED, 8 DO, 24V DC, 0.5 A (1 X 8 DO), SHORT-CIRCUIT PROTECTION, DIAGNOSTICS, 20 PIN 6ES7322-8BF00-0AB0 Do these 2 modules work the same? or are there any differences? With the combination of the 2 modules, I have enough DO for my project. Can someone give some advise? Thanks! Berre |
| 2/16/2006 8:33 PM | |
|
Joined: 9/23/2005 Last visit: 1/9/2026 Posts: 4443 Rating:
|
Hi, Detailed information’s about this module are in the manual: http://support.automation.siemens.com/WW/view/en/8859629 The front connector, the total current and the parallel connectivity capacity are different. |
|
Denilson Pegaia |
|
Follow us on