4/28/2008 12:36 PM | |
Joined: 4/6/2006 Last visit: 2/5/2024 Posts: 604 Rating: (56) |
Hi, I think that your answer is answered in the folowing FAQ. There is described that 3 HMI's are possible for a 226. The most interesting part is the 2nd table which shows al the numbers combined with baudrates. Which HMI components can you connect with S7-200 CPU and what should you watch out for when doing so? |
Best regards, |
|
4/28/2008 1:34 PM | |
Joined: 5/8/2006 Last visit: 4/29/2024 Posts: 1085 Rating: (77) |
Hi, you can connect all three panel to a S7-200 PLC with a standard MPI or Profibus cable. You onlyneedthe SIMATIC S7 communication driver in WInCC flexible. If both panels have an ethernet port you can use Sm@rtAccess via ethernet. Bars and gauges arestandard objects of WinCC flexible. If thevalue in plc not theright display value you can changevalue by the linear scaling of the tag. You find the options in the properties of the tag. Bye |
Follow us on