9/22/2017 11:05 AM | |
Posts: 86 Rating:
|
Hello all, Recently i'm facing a little problem with KTP900 Basic 2nd generation. programming with TIA Pro V14. I created an alarmview screen and also a template that the bottom of the screen is alarmview as well, offline all seems to be right the application is compiled without any errors but when i simulate it or download to the panel the alarmview widget invisible. Alarms are defined as digital alarms, in plc the alarms saved in DB as word. i configured them as well as word from DB and selected first 2 bit(bit0 and bit1). i even checked that i get this values and all seems to be right except that the widget are invisible. attaching few screenshots(the screens are archived with rar the .doc shall be .rar). Thanks in advance, Attachmentscreens.doc (37 Downloads) |
Follow us on