6/27/2017 1:49 PM | |
Posts: 1 Rating: (0) |
hello i have problem with connecting logo! with pc my error is attached below plz who can help me ------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 6/27/2017 2:01:39 PMNew subject after splitting |
|
6/27/2017 1:55 PM | |
Joined: 12/18/2014 Last visit: 9/27/2024 Posts: 33843 Rating: (4206)
|
Is the LOGO! new? Is it a LOGO!8.FS04? Then may help this FAQ: Why can you not download any programs into your new LOGO! 8? |
6/28/2017 9:00 AM | |
Joined: 2/20/2014 Last visit: 9/17/2024 Posts: 396 Rating: (38) |
Is your hardware selection done correctly at the LOGO Soft Comfort? Did you choose the correct network card (i notice you have selected the wireless network card). What is your connection method from PC to LOGO? Is the PC & LOGO connected via a wireless router or through LAN cable? Is your PC IP address is in the same range as the LOGO device? Is your LOGO device the latest? (FS.04)
|
Follow us on