4/2/2018 11:51 AM | |
Posts: 2 Rating: (0) |
dear sir you can you make example about control motor speed ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 4/3/2018 9:16:30 AMNew subject after splitting |
|
4/3/2018 11:05 AM | |
Joined: 11/14/2008 Last visit: 5/6/2024 Posts: 504 Rating: (22) |
Hi, Here in this link you can filter for an application example... https://www.automation.siemens.com/mc-app/sinamics-application-examples/Home/Index?language=en |
4/4/2018 2:24 AM | |
Joined: 10/25/2016 Last visit: 9/1/2022 Posts: 199 Rating: (25) |
Hi, More details please, you want to control the speed of what? a Motor? if you want control the speed of motor what kind of motor is it? Alternative current or continue current? in case of alternative current is it 230 or 480 or 400 volt? do you want control the speed using drive or other? You got many way to control the speed, this is also depending of the Power of the motor, you don't control the speed of 24 Volt Continue current Motor such as 480 Volt Alternating current motor. Regard |
This contribution was helpful to1 thankful Users |
Follow us on