7/2/2018 11:07 AM | |
Posts: 3 Rating:
|
Hello, i'm having a little issue with the Stand Alone („Ready-for-use“ for legal-for-trade stand-alone operation without SIMATIC CPU) project. I've downloaded the whole project, managed to make the WP251 communicate with the TP700. So my legal-for-trade display is loaded and working. The only problem I have now is whenever I try to send a command ( >0<, TARE, higher resolution, ...) the HMI is saying: "tag WP251_SCALE_1_s_CMD2_bo_CMD_TRIGGER that the value can not be written to the PLC". Wich is kinda logical since i'm not using any PLC. How can I make sure the commands get through and let the WP251 get on zero for example by pushing a >0< button? Is there anything to be changed to the script? Or is it something else? The components I use is: TP700 Comfort WP251 Thank you in advance. |
Last edited by: Jen_Moderator at: 7/3/2018 7:48:04 AMOptimized link. |
|
Follow us on