12/22/2018 11:42 AM | |
Posts: 7 Rating:
|
Hello! I have problem with communication between PC to CMR on VPN tunel I use this solution Setting up a Secure VPN Connection between a PC and LOGO! 8 My CMR 2020 Activated firmware version V2.1.5 Bootstrap version V1.1.4 Mobile wireless module version 13.00.106 Connection established : YES Connection to data service established : Yes (GPRS) When CMR logs into the mobile network I have public IP I use Automatic time-of-day synchronization, via NTP works fine Then I Setting up remote access according to point 2.3 in this document I don't use DynDNS so I modify vpnpeer.conf by replace the DynDNS entry in line 4 by my public IP address. Save file cmr.ovpn On PC I use OpenVPN v 2.4.6 import my cmr.ovpn file and connect The OpenVPN client never establishes a VPN tunnel to LOGO! CMR bytes is send but not receive I'm doing something wrong or problem is in the other things Regards |
3/19/2019 2:56 PM | |
Posts: 3 Rating:
|
Hi, I'm stuck at the same point... Have you resolved your problem ? Thanks ! Jérémy |
Follow us on