3/23/2019 11:11 AM | |
Posts: 2 Rating: (0) |
>hello everyone, I find a problem with the application LOGO! App I established the communication without any problem but I can not monitor the analog value of the analog input it is still 0 even if I vary the analog input from the program is what there is someone who has the same problem ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 3/25/2019 7:49:30 AMEdited text for better reading. Last edited by: Jen_Moderator at: 3/25/2019 7:50:30 AMNew subject after splitting |
|
3/24/2019 9:06 PM | |
Posts: 2 Rating: (0) |
38 and i have 0 in the app logo even if the communication is istablished |
Follow us on