8/27/2019 1:24 PM | |
Joined: 12/18/2014 Last visit: 6/28/2024 Posts: 33250 Rating:
|
For Modbus TCP/IP you need at least one LOGO! 0BA8 with the production status FS:04. Product information on LOGO! 8 FS:04 and FS:05 In addition, I would install the current software version LSC V8.2.1. You can download the update here: But it is a big complete package with other software (1,3 GB). And the included firmware update is not for your LOGO!. The setting whether the LOGO! works as a server (slave) or master (client), you set it in the connection settings. |
8/27/2019 2:04 PM | |
Posts: 2 Rating:
|
I have 6ED1052-2MD00-0BA8 some one say that I need 6ED1052-2MD08-0BA8 It's true? |
Follow us on