9/24/2019 7:51 AM | |
Joined: 11/14/2018 Last visit: 7/26/2024 Posts: 502 Rating:
|
Hello Desert Monkey, i'm not sure, if I understood you correctly. If it's the last case, then I can say, that I also have no analogue gauge in my toolbox, if I work with basis panels. Greetings, Nzett11 |
If I could help you, be so kind and rate my contribution. :) |
|
9/25/2019 6:58 PM | |
Joined: 2/24/2015 Last visit: 1/25/2023 Posts: 306 Rating:
|
Gauges are available in Comfort panels (which are programmed in WinCC Comfort). You can download the HMI Toolbox library - there is a gauge element there. This is not exactly a gauge - a graphic list with 100 pictures. But you can use it. |
9/29/2019 9:48 AM | |
Joined: 2/29/2016 Last visit: 9/4/2024 Posts: 40 Rating:
|
Hi All Thanks for the information guys, I will start to save for the upgrade for winCC |
Follow us on