11/12/2019 10:21 AM | |
Joined: 11/6/2019 Last visit: 3/13/2022 Posts: 5 Rating:
|
OK Guys, a further Question if I may.... The TP177A Panels are now working, But we have a TP177B PN/DP Panel, When I try to back this up using ProSave, the Backup Option is "greyed" Out when I I have selected the correct Panel/USB PPI/Cable from the General Option TAB of ProSave, When I select the Top connection of Serial RS232 multimaster Cable, the backup Option is available? Does this mean that I cannot use the recently purchased USB/PPI Cable for a TP177B Panel? or have I missed a setting somewhere in ProSave? TIA for any further assistance that someone could provide.... ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 11/12/2019 13:41:55New subject after splitting |
|
Follow us on