11/16/2019 10:38 PM | |
Joined: 10/28/2017 Last visit: 5/19/2024 Posts: 1 Rating:
|
Hello, I have C7 626, previously I added another HMI MP177 6" and I migrated it with wincc flexible 2008. Now, the PLC is good, but i think the HMI doesn't boot (i cannot see inside,the hmi lost all its luminosity) my problem is at startup by default the HMI force the cpu at stop mode. and the function to start the CPU from MP177 6" is not available. can you help me to start the cpu without the C7 626 HMI Best regards. Dj@mel ------------------------------------------------------------------------------------------ |
Last edited by: Dj@m at: 11/16/2019 22:41:46Last edited by: Jen_Moderator at: 11/18/2019 07:31:33New subject after splitting |
|
Follow us on