3/7/2020 10:28 AM | |
Joined: 3/6/2020 Last visit: 5/16/2024 Posts: 7 Rating: (0) |
Hi again.. If we consider a 100,000 write cycle for the MMC and our panel storing logs data 5 times per second this mean the life service of the MMC will be affected strongly in just few hours or days, is that reasonable? or I misunderstand something? Thank you |
3/8/2020 7:32 PM | |
Joined: 5/28/2008 Last visit: 11/6/2024 Posts: 4516 Rating: (839) |
Hello, 100,000 write cycles is for MMC which we use in S7 300 CPUs. And these type of Micro Memory Cards are not suitable for comfort panels. Which external storage media can you use with the current SIMATIC panels and which memory card interfaces do they have? |
Ayman Elotaify |
|
3/8/2020 8:09 PM | |
Joined: 3/6/2020 Last visit: 5/16/2024 Posts: 7 Rating: (0) |
Hello and thank you for your replay: comfort panel can accept commercial MMC cards (e.g SanDisk MMC cards) for data logs but even those cards have a limited number of write cycles and for 0.2Hz writing frequency (write cycle every 5 seconds) we still have a few days or even few weeks before MMC life service ends, my question is can I change this writing time or not because I want to archive data from PLC every hour and not every 5 seconds (I know that I can select the acquisition time for the data log ) but does this also change the 0.2Hz writing frequency of the panel or its a fixed number? Thank you again |
3/9/2020 12:19 PM | |
Joined: 4/26/2012 Last visit: 11/5/2024 Posts: 1560 Rating: (169) |
Hello, can you explain better how you are doing the log writing? What programs and device are you using? |
"Always make a backup before and check the best time before testing." |
|
3/9/2020 8:21 PM | |
Joined: 3/6/2020 Last visit: 5/16/2024 Posts: 7 Rating: (0) |
Hi I am using TIA portal v15.1 to write an HMI program for comfort panel TP1200 and I used a circular data log with one hour logging cycle but I get confused when I read in the comfort panel operation instruction manual that the panel stores log data in a frequency of 0.2Hz and that makes me ask about the lifetime of the MMC card and which cycle time the panel will use. |
Follow us on