8/24/2020 11:05 AM | |
Joined: 2/22/2008 Last visit: 8/6/2024 Posts: 2698 Rating: (208) |
See example for multi networking with Logo's. Maximal 32 Logo controller can be inserted in a network diagramm. They can be sorted in groups as you need. One Logo is defined as master (in the example Group 1 Server) You just need a plan for VM mapping without overlap. In Access Tool and advanced Webserver you don't need any network inputs to read the status of all Logo controller inputs and outputs. You only need network inputs to handle inputs/outputs from Logo x in Logo y. The example is only a schema without logical programs. Regards, Scorp AttachmentMultinet1.zip (232 Downloads) |
This contribution was helpful to1 thankful Users |
Follow us on