2/24/2021 5:44 PM | |
Joined: 7/5/2013 Last visit: 10/2/2024 Posts: 3114 Rating: (512) |
Hi,
several drivers are installed on the panel and mostly it is up to the setting to get e.g. a PCLx printer running. Have a look in the following download entry: Commissioning of approved printer for SIMATIC HMI Panels It is possible to use non-approved printers with the same settings as approved printers. Siemens just didn't test each available printer. Regards, Frink |
Pi is exactly three! |
|
Follow us on