2/1/2017 9:44 PM | |
Joined: 9/3/2008 Last visit: 11/4/2024 Posts: 928 Rating: (163) |
Hi, The max number of connections you can create are 8. See the manual SIMATIC HMI HMI Devices Comfort Panels In paragraph 8.10 it describes the number of connections. In your project, when you have both the cpu and the panel and create an HMI connection between them, they information about address is automatically known. Then you can just access the PLC tags from the WinCC project. |
Michael |
|
This contribution was helpful to2 thankful Users |
Follow us on