5/7/2021 8:10 AM | |
Joined: 4/21/2021 Last visit: 3/22/2022 Posts: 6 Rating:
|
Hi I work on a car lift that I have some challenges with. Overview: When I6 + 7 is high, the lift is at the bottom. Q1: Hydraulic pump (lifting) I have made a counter function which starts the warning sound when it is at a certain height, 150mm. What I need help with: AttachmentLDI Prog.zip (754 Downloads) |
Last edited by: AMR-AC-HYDRAULIC at: 05/07/2021 08:26:15Last edited by: AMR-AC at: 05/07/2021 09:35:41 |
|
5/7/2021 8:13 AM | |
Joined: 6/19/2019 Last visit: 9/5/2024 Posts: 697 Rating:
|
Hello, First add your program to help you. |
5/7/2021 8:27 AM | |
Joined: 4/21/2021 Last visit: 3/22/2022 Posts: 6 Rating:
|
Now added :-) |
5/7/2021 9:10 AM | |
Joined: 6/19/2019 Last visit: 9/5/2024 Posts: 697 Rating:
|
Please also add .zip format program |
5/7/2021 9:35 AM | |
Joined: 4/21/2021 Last visit: 3/22/2022 Posts: 6 Rating:
|
Done :-) |
5/8/2021 7:35 PM | |
Joined: 4/14/2013 Last visit: 7/17/2024 Posts: 32 Rating:
|
Hello. The best... E: |
Last edited by: erku at: 05/08/2021 19:48:18Last edited by: erku at: 05/08/2021 19:56:26 |
|
5/10/2021 7:09 AM | |
Joined: 4/21/2021 Last visit: 3/22/2022 Posts: 6 Rating:
|
Hello! In Europe we don't have a requirement of a mechanical locking. Our standard says, that we should be able to handle one hydraulic leak. This lift is a two pillar underground with one cylinder in each pillar, so one cylinder and the mechanical structure are able to carry the entire load, with a maximal drop of 100mm. The standard says, that our main switch can replace a EMG switch. And then to your question. The lift should stop at a specific height (danger of squeeze). And then it should be allowed to lower entirely. |
Last edited by: AMR-AC at: 05/10/2021 07:22:39 |
|
6/3/2021 9:37 AM | |
Joined: 4/21/2021 Last visit: 3/22/2022 Posts: 6 Rating:
|
Anyone who can help me? I work on a car lift that I have some challenges with. Overview: Q1: Hydraulic pump (lifting) I have made a counter function which starts the warning sound when it is at a certain height, 125mm. What I need help with: Thanks :-) AttachmentLIFT.zip (796 Downloads) |
Follow us on