3/12/2019 3:00 PM | |
Joined: 4/6/2017 Last visit: 6/16/2022 Posts: 69 Rating: (1) |
Nothing happens if I click double arrow. No error messages, no LOGO! appears in the list, nothing. |
3/12/2019 3:01 PM | |
Joined: 4/6/2017 Last visit: 6/16/2022 Posts: 69 Rating: (1) |
The list remains empty. |
3/18/2019 2:09 PM | |
Joined: 4/6/2017 Last visit: 6/16/2022 Posts: 69 Rating: (1) |
I read somewhere that IP may be 192.168.0.203. |
3/18/2019 2:31 PM | |
Joined: 4/6/2017 Last visit: 6/16/2022 Posts: 69 Rating: (1) |
I could not change the IP address. I just tried with 192.168.0.203 too? |
3/18/2019 2:44 PM | |
Joined: 2/22/2008 Last visit: 5/10/2024 Posts: 2698 Rating: (206) |
You also can use a little ip scanner, if you have problems to find a device. I often use this scanner Link See attached picture of a possible result of the scanner. Networks are not easy, if there is a little fault in the configuration. You need the right ip adrress, right subnet mask and pay attention, not to use an ip address a second time. These are only the main objects to mind. Regards, Scorp |
This contribution was helpful to1 thankful Users |
3/18/2019 2:48 PM | |
Joined: 4/6/2017 Last visit: 6/16/2022 Posts: 69 Rating: (1) |
Here is the screenshot with ipconfig /all. |
3/18/2019 3:15 PM | |
Joined: 12/18/2014 Last visit: 5/11/2024 Posts: 33008 Rating: (4078)
|
Can it be that a firewall is blocking the ports? Have you ever turned off the Firewall? |
3/18/2019 3:29 PM | |
Joined: 12/18/2014 Last visit: 5/11/2024 Posts: 33008 Rating: (4078)
|
Can you ping the LOGO! ? ping 192.168.0.3 |
3/18/2019 5:05 PM | |
Joined: 12/18/2014 Last visit: 5/11/2024 Posts: 33008 Rating: (4078)
|
Attached is an excerpt from the manual of the current LOGO! 8.2. It's about network security and which ports the LOGO! used. AttachmentLOGO! 8 manual 0BA8 2017_11 xxxx8-0BA0 pages 301-303.pdf (212 Downloads) |
3/19/2019 8:50 AM | |
Joined: 4/6/2017 Last visit: 6/16/2022 Posts: 69 Rating: (1) |
Thank you for the manual, Ixo65. It is very useful in my battle with IT guys. |
3/20/2019 3:06 PM | |
Joined: 12/18/2014 Last visit: 5/11/2024 Posts: 33008 Rating: (4078)
|
Not in my opinion. If I were in your place, I would start a Support Request. |
3/21/2019 7:24 AM | |
Joined: 4/6/2017 Last visit: 6/16/2022 Posts: 69 Rating: (1) |
Hi Scorp, I tried your IP scanner too. No result. I connect just PC and LOGO!, no other network. |
3/21/2019 8:46 AM | |
Joined: 12/18/2014 Last visit: 5/11/2024 Posts: 33008 Rating: (4078)
|
Did you follow my suggestion and start a Support Request? |
3/21/2019 9:54 AM | |
Joined: 4/6/2017 Last visit: 6/16/2022 Posts: 69 Rating: (1) |
Not yet. I will try now support request. |
3/21/2019 11:52 AM | |
Joined: 4/6/2017 Last visit: 6/16/2022 Posts: 69 Rating: (1) |
I sent the support request. |
3/21/2019 11:53 AM | |
Joined: 4/6/2017 Last visit: 6/16/2022 Posts: 69 Rating: (1) |
I sent the support request. |
3/22/2019 12:14 PM | |
Joined: 4/6/2017 Last visit: 6/16/2022 Posts: 69 Rating: (1) |
I bought it as new one. It was in original package. But this is not so important now. |
3/22/2019 3:11 PM | |
Joined: 12/18/2014 Last visit: 5/11/2024 Posts: 33008 Rating: (4078)
|
Attached a screen video.
AttachmentIP scanning with LSC.zip (196 Downloads) |
3/22/2019 3:30 PM | |
Joined: 12/18/2014 Last visit: 5/11/2024 Posts: 33008 Rating: (4078)
|
I wish you also. |
Follow us on