3/9/2017 5:13 PM | |
Posts: 1 Rating: (0) |
Hello All,
I have a Industrial PLC running Windows RT, and is a propreitory development of my company. The system can network through CAN, EtherCAT, Serial etc. and is used to control AC motor inverters, and other I/Os. We have to control a 3-phase motor via this control system. The motor has a built-in inverter, and a HMI panel integrated in the body for basic controls such as ON/ OFF, speed increase/ decrease, rotation direction.
Please advise if/ how this can be achieved, in normal cases? Also if we can get any peripherals to get this done. Thanks. ------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 3/13/2017 2:05:33 PMNew subject after splitting |
|