2/21/2019 1:43 PM | |
Posts: 1283 Rating: (105) |
Is this format you are mentioning which we can select in LOGO or the Modbus device? |
2/21/2019 2:51 PM | |
Joined: 2/22/2008 Last visit: 8/6/2024 Posts: 2698 Rating: (208) |
Maybe you receive something, but not every bit pattern is a valid float number. You need at least 2 words (4 bytes) for Float, or 4 words (8 bytes) for Double. In the data table chose VD0 and hexadecimal representation, also add VD4, VD8 and change incomming parameters for more words. For float you can check the incomming bit pattern or hexadecimal representaion on the following page. https://www.h-schmidt.net/FloatConverter/IEEE754.html Upload a Modbus implementation table from inverter, mostly added with information of the number format to get more help. Regards, Scorp |
Last edited by: Scorp at: 2/21/2019 2:54:35 PM |
|
This contribution was helpful to1 thankful Users |
Follow us on