8/10/2015 4:16 PM | |
Joined: 12/18/2014 Last visit: 8/7/2024 Posts: 33500 Rating: (4162) |
Then must be the analog mux available in the analog folder. |
8/12/2015 9:40 AM | ||||||||||||||||||||||||||
Posts: 5 Rating: (0) |
Excellent! Thank you very much. I upgraded the program yesterday, the sensor went from always reading 1 Bar to reading 0.004 Bar with a Analog Threshold Value of 2. The vacuum pump would run for the entire motor on time. I've attached the program, i think either I've chosen the wrong sort of sensor, or it's a bad sensor. The sensor details are: Make: Gems Sensors Model: 3300R01B0G01B000
I choose this sensor, as i needed one to go to max 1 bar and read to 0 bar, it needed to be voltage regulated for the Logo!. I read that Gauge type was the correct sensor for my application. Is this correct? The main program is on the plc called Biltong_Live. Hope you can help! Thanks again for your support thus far. Andrew AttachmentBiltong.zip (322 Downloads) |
|||||||||||||||||||||||||
Follow us on