2/21/2023 1:26 PM | |
Joined: 1/13/2023 Last visit: 3/11/2024 Posts: 2 Rating: (0) |
Hi, I have the same task: Control a 3-way valve with 3 Point valve actuator. I need to control it with PXC100-E.D. using two DO - one for opening and one for Closing. It works the same principle: when the signal for valve opening is active, the valve starts to open. Once the signal is inactive, the valve stops in position. The same way for closing You can see the attached connection diagram. The question: is there any FB to control this type of actuator like you have mentioned PID_3step? In case if not: what are my options? Do I have to create a virtual position of the actuator using stroke and running time? ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 02/22/2023 11:17:24New subject after splitting |
|