2/20/2016 6:53 PM | |
Joined: 1/17/2006 Last visit: 2/7/2022 Posts: 171 Rating: (0) |
Hi expert, AttachmentXMLLog.txt (170 Downloads) |
2/21/2016 11:06 AM | |
Joined: 6/23/2008 Last visit: 10/17/2024 Posts: 1168 Rating: (282)
|
Hello munneb, when checking your log-file I saw already that drivers for a CPU 416-3 DP and on other CPU 417-4H should be generated...I couldn't understand because I have never seen a configuration with two CPUs on one rack. I am sorry to say, but I think you should ask now Siemens Customer Support and open a Service Request. Or maybe some other users can help here, but I think this is a very special case. I wonder how this can work...Please tell me; Does each CPU (of AS1) has an own S7-program? Anyhow, it would be very interesting how this issue is solved at the end, so please, share it here! Best regards... P.S.: Also I saw now that the rack 6ES7 401-2TA01-0AA0 is not released for PCS7 V7.1 (and I guess also not for other versions). Please see this document for V7.1. If you are on the profile PCS7 V... in HW-config you can see that there is no rack availble where you could place more than one CPU in one rack (The rack for H-Systems are physically two racks). So I think your configuration is not a propper PCS7 configuration. I think the people whow created this project did something on the ES to avaoid generatin module drivers for the CPUs. I can imagin what they did but before I would like to know something; Could you please compile the entire program in V6 and share the full protocol 'Module Drivers' (use 'Save') here? |
Last edited by: mark1507 at: 2/21/2016 11:24:36 AMLast edited by: mark1507 at: 2/21/2016 11:41:40 AMLast edited by: mark1507 at: 2/21/2016 12:14:56 PM"Expert" does not necessarily mean Siemens employee. Please cross-check your requirements always with official Siemens documentation. Also "Experts" are pleased about feedback. Please don't send support requests as PM. Questioners who don't follow up their thread will be put to my list of users to be ignored. |
|
2/21/2016 1:37 PM | |
Joined: 6/23/2008 Last visit: 10/17/2024 Posts: 1168 Rating: (282)
|
Hello muneeb, Yes, you could go like this, but take the correct (released) racks for both CPUs... honestly said; I would even try to convince the customer to spend a little bit more money and replace the 18-slot rack by two 9-slot racks wich are suitable (see document Released Modules Vx.y) for PCS7. The advantage would be a better support of the 'driver wizard' what will result in a higher level of diagnosis. Also, I think the @CPU_RT chart, wich is autmatically generated by the system from version V7.0 on, will be available only in that case. If you like to know what the advantages of the chart @CPU_RT are, see this article. Maybe you have to update the firmware of the CPUs for using the functionallity of the @CPU_RT chart. You can find out here. What kind of racks are used for AS2 and AS3 ? Anyhow, I guess even on the ES in V6 you actually have some warnings "CPU xyz is not supported" in tab 'Module drivers' because your predecessors disabled something in the ES to compile without errors (but warnings). I also think I know what they did.... Would be nice if you could share that V6 protocol here... Best regards... |
Last edited by: mark1507 at: 2/21/2016 1:39:28 PMLast edited by: mark1507 at: 2/21/2016 1:42:49 PM"Expert" does not necessarily mean Siemens employee. Please cross-check your requirements always with official Siemens documentation. Also "Experts" are pleased about feedback. Please don't send support requests as PM. Questioners who don't follow up their thread will be put to my list of users to be ignored. |
|
Follow us on