3/24/2020 6:30 PM | |
Posts: 6 Rating: (0) |
Hello! I wrote a small test program for LOGO ! and created a visualization for it. Both the program itself and the visualization were downloaded to LOGO! without mistakes. When starting visualization through a browser (chrome), there is no any picture (background and buttons) exept for text, so there is no way to push buttons and watch anything. Accordingly, the tail of the menu and itself is not there either. I climbed into the browser settings, allowed this site all the pictures, flash and javascript, but that didn't help either. If you start pages from the folder saved by the project from the computer, then everything is displayed perfectly. I looked at F12, heaps of errors, and each time when i start visualization, they are different. It feels like something setting arbitrary changes to javascript every time, and the browser is lost. What could be the problem? It should be: [snip] What is visible: [snip] When I restart visualization: [snip]
Attachmentimages.zip (137 Downloads) |
Last edited by: Jen_Moderator at: 03/25/2020 06:06:33Removed links and added files as an attachment. |
|
3/24/2020 8:15 PM | |
Posts: 6 Rating: (0) |
Of course, the projects in the attachment. I have LOGO! 230RC 6ED1052-1FB08-0BA0, Firmware version 1.82.02 The version of LOGO! Web Editor is V1.0.1 AttachmentVisual_test.zip (118 Downloads) |
3/24/2020 8:49 PM | |
Joined: 12/18/2014 Last visit: 5/27/2024 Posts: 33113 Rating: (4088)
|
I tested it with 4 Browsers. With all 4 browsers the function is given. - Internet Explorer 11 AttachmentWeb Server.zip (133 Downloads) |
3/24/2020 9:51 PM | |
Joined: 12/18/2014 Last visit: 5/27/2024 Posts: 33113 Rating: (4088)
|
Good question, but it's not easy to answer. Maybe you should start a Support Request. |
3/24/2020 9:55 PM | |
Joined: 12/18/2014 Last visit: 5/27/2024 Posts: 33113 Rating: (4088)
|
In attachment my test projects. Try this.... AttachmentWeb editor test.zip (136 Downloads) |
3/24/2020 11:38 PM | |
Posts: 6 Rating: (0) |
I've done all your steps, but this still doesn't work( Another computer has Windows 7, just in case. |
3/24/2020 11:40 PM | |
Posts: 6 Rating: (0) |
Tried your example, it doesn't work properly too( Wrote to Siemens Support, waiting for their reply |
Follow us on