5/10/2025 7:15 PM | |
Joined: 9/13/2012 Last visit: 9/4/2025 Posts: 27 Rating:
|
Hello . I want to change control from contactor to inverter for pump. I am working with 315PN-DP controler, 6SL3210-1KE21-7AF1 with software Step7 V5.6 and Simotion Scout V5.4 . I ve added drives in step/scout few times but mainly DP type. Today I am trying to add PN drive. I watched the movie showing proces. https://www.youtube.com/watch?v=JPDfO9iv6E8 When i get to the point (8:20 )where after assigment of IP I should connect to the drive but I am reciving error that connection is not possible. I see that I can ping unit from PG, when I disconnect profinet cable both PLC and VFD gives communication errors so it looks that it is open for communication . I can upload drive from online device to Scout project but can not assign drive as declared in step 7 new drive. I ve tested connection with Device/USB but after marking found drive in accesible nodes and getting in connect online drive i get window with inactive newly created PN drive , only possible to mark other DP drive... with red color that it is wrong selection. When I try to do this via profinet i get just error: Connect to selected target device not possible. As mention i ve did configuration as in movie. I did assigment of unit name and ip adress in step7 , same in scout... checked few times connection between scout , device but ...without success. Any advices what am I missing? Sorry I cant add second picture - some limit in the forum. |
Last edited by: Icos13 at: 05/10/2025 19:16:29Last edited by: Icos13 at: 05/10/2025 19:31:45Last edited by: Moderator_Lan at: 05/12/2025 08:42:47Video embedded. |
|
5/12/2025 9:26 AM | |
Joined: 5/12/2006 Last visit: 9/2/2025 Posts: 22709 Rating:
|
are you direct connected to the G120? |
Follow us on