9/8/2025 8:25 PM | |
Joined: 4/19/2025 Last visit: 9/11/2025 Posts: 2 Rating:
|
HI, I have a project with a CU240E-2 PN-F and PM240-2 IP20 that has r2 = 44 switch on inhibited-supply STO terminal w/24V (hardware). I have no idea why it's throwing this error! STO is not active in this project. I attached the project I downloaded to the VFD. It threw this error after I swapped the CU between two panels to debug a different issue. Swapping the CUs back didn't help. I appreciate any insight! I measured 24V in these pins and 0V as noted. AttachmentError.zip (4 Downloads) |
9/9/2025 11:34 AM | |
Joined: 4/19/2025 Last visit: 9/11/2025 Posts: 2 Rating:
|
Please, if anyone could lend an insight into this, I'd appreciate it greatly |
9/16/2025 9:28 AM | |
Joined: 9/21/2012 Last visit: 9/17/2025 Posts: 4714 Rating:
|
Try reseting the drive back to factory settings and download the parameters again after that. |
Follow us on