6/14/2013 2:32 PM | |
Posts: 215 Rating: (6) |
Hello BryanG2001, did you look up the following entry as a reference? http://support.automation.siemens.com/WW/view/de/41127453? If it is not helpful, what about to post some specifications of your configuration here as well as the complete program? Maybe thesupply of the interface causes problems. Best regards |
6/17/2013 9:40 AM | |
Posts: 215 Rating: (6) |
Hello BryanG2001, the manual regarding high speed counters specifies that more than one HSC can be run at one time no matter which type of CPU you are using. The behavior of your HSC seems to differ to that. I think you are able to apply the HSC in the right way because you are experianced with this matter. So I would recommendyou to ask the siemens technical support for help. http://support.automation.siemens.com/WW/view/en/4000024+16605032 http://support.automation.siemens.com/WW/view/en/16605656 Best regards |
6/17/2013 3:34 PM | |
Posts: 113 Rating: (22) |
Thank you for the links, I will have to give Siemens Support a try. |
Follow us on