4/8/2021 7:36 PM | |
Joined: 4/14/2016 Last visit: 5/21/2024 Posts: 10 Rating: (0) |
Let me explain: I have like 6 languages in HMI, they work fine. When I select another language all the texts are changing to that specific language. But I want not to specify my alarms in the HMI but in de PLC. So I've tested it with program alarms. When you select those languages in the PLC hardware config they are also multi language in the HMI. But only 3 of them :( This principle in explained here: https://support.industry.siemens.com/cs/ww/en/view/109759021 I only want the program alarms in 6 languages in the HMI. The alarms at the webpage or lcd screen are a "nice to have" for me. |
Last edited by: Jen_Moderator at: 04/09/2021 08:59:29Optimized link. |
|
4/8/2021 11:44 PM | |
Joined: 7/7/2010 Last visit: 5/17/2024 Posts: 14751 Rating: (2374)
|
I found the F1-help reference to what you are using: Central Alarm Management in the CPU Here's the part you are painfully already aware:
So, to get what you want, you need some automation (scripting, like TIA Openness can do) to export your PLC texts in >3 languages, mate them up with HMI based alarms and push the texts into those alarms. With some rigid structure (conventions) you could get that working pretty quickly semi-manually with exports & imports.
|
science guy |
|
4/12/2021 7:39 AM | |
Joined: 4/14/2016 Last visit: 5/21/2024 Posts: 10 Rating: (0) |
Ok, I tought maybe there's a method to get more languages to the PLC. If you read the help they say this: "number depends on the CPU". Is there any method to create automaticly HMI alarms when you connect a HMI-tag to a specific PLC-object?
|
Follow us on