2/23/2009 7:01 PM | |
Joined: 3/21/2006 Last visit: 9/10/2024 Posts: 10228 Rating: (1181) |
Hello Look at Which SIMATIC NET PROFIBUS PC CP is compatible with which operating system? . First possible choice CP5611. Different is that this card is PCI not ISA. And also you must use data traffic with a data length of 9 bytes or more. Other choice CP5613. (not A2). But this card is old product, I don't suggest you to buy. This is PCI card. Unfortunatly, I don't think that you can use directly this card without make any changes in software. regards |
Follow us on