6/14/2021 2:35 PM | |
Joined: 10/18/2006 Last visit: 7/9/2024 Posts: 120 Rating:
|
Hi AutoGen_7421556, based on the information you wrote, it is hard to give you an advise, because according to the used interface different causes are possible. In a first step please double check with STEP 7 VAT or the online view that the signals are really set simultanously. If you still need assistance please contact directly your local iba AG representative, which can be found here. |
iba AG - Data Acquisition and Analysis the way it should be |
|
This contribution was helpful to
1 thankful Users |
6/16/2021 10:40 AM | |
Joined: 10/18/2006 Last visit: 7/9/2024 Posts: 120 Rating:
|
Hi, since the blue and the red signal are missing for almost 1s, I won't expect any difference when using a Profibus monitor instead of the S7-Xplorer interface. Or is the update time very high, > 500ms? Are you sure that the red and blue signals are not overwritten somewhere else in your program? And it would also be a good approach to add a new (100% surely unused) memory bit and apply it in the same way. Would be interessent how long it will stay set. |
iba AG - Data Acquisition and Analysis the way it should be |
|
Follow us on