3/20/2022 11:11 PM | |
Joined: 6/20/2020 Last visit: 3/22/2022 Posts: 1 Rating: (0) |
I am also having issues with Kepware. I am reading a quite long DB and only the last 4-5 real values (out of a couple of hundred and a number of BOOL) are tagged as BAD quality. I have read in other forums that there might be a limit on the DB length but I cannot find which is this limit for OPC UA and Kepware. Can someone please comment? Thanks ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 03/21/2022 12:05:09New subject after splitting |
|
3/22/2022 7:13 AM | |
Joined: 3/11/2019 Last visit: 7/9/2024 Posts: 1511 Rating: (270) |
Hi Tomcat_ar1973, i do not know any limitations about Kepware, but as for OPC UA on S7-1200/1500, there is following FAQ. Maybe it is helpful. What are the system limits of the OPC UA Server with S7-1500 and S7-1200?regards sancruz |
Feedback appreciated, please rate |
|
This contribution was helpful to1 thankful Users |
Follow us on