9/23/2014 1:08 PM | |
Joined: 3/20/2013 Last visit: 4/3/2024 Posts: 676 Rating: (44) |
You need a SIMATIC NET Software which can be installed on your windows system. The CP5711 in general is compatible with win7 32bit. http://support.automation.siemens.com/WW/view/en/22611503 you have to install e.g. SIMATIC NET V12 |
Best Regards, |
|
This contribution was helpful to1 thankful Users |
5/11/2022 10:56 AM | |
Joined: 2/23/2022 Last visit: 5/20/2022 Posts: 2 Rating: (0) |
Hello, I have same issue. Is somebody find driver for CP5711 or what can I do? thanks in advance, Br, Mario |
5/17/2022 1:32 PM | |
Joined: 2/23/2022 Last visit: 5/20/2022 Posts: 2 Rating: (0) |
Thanks for help, I install driver with Simatic NET, but still i have some erorr, CODE10. BR, Mario |
5/17/2022 3:30 PM | |
Joined: 3/11/2019 Last visit: 11/8/2024 Posts: 1653 Rating: (305) |
Hi, after you have installed SIMATIC NET software, please reinstall the driver manually via folder "C:\Program Files\Common Files\Siemens\Automation\Simatic OAM". Please have a look at following FAQ (even if this FAQ is for USB adapter), but this should work for CP5711 as well. How do you update the driver software for the PC Adapter USB if you cannot establish an online connection after installing STEP 7 (TIA Portal)?maybe this helps regards sancurz |
Feedback appreciated, please rate |
|
Follow us on