7/19/2022 12:36 PM | |
Joined: 7/9/2015 Last visit: 11/19/2024 Posts: 4028 Rating: (603)
|
Hi, Inputs of a module can be read by both PLCs but outputs can only be written by one CPU and only read by the second CPU. So for outputs, only one CPU can have write access. Also please check this FAQ: How, in STEP 7 (TIA Portal), do you configure access to a shared device and the function Module-internal Shared Input / Shared Output (MSI /MSO)?Regards, Towome |
|
|
This contribution was helpful to1 thankful Users |
7/26/2022 6:35 AM | |
Joined: 5/11/2022 Last visit: 11/6/2024 Posts: 64 Rating: (0) |
is there anyway to change write access of PLCs? can you help me how I can create control logic to have both PLCs able to control it by having one PLC control it unless a remote request comes in from the 2nd PLC that says to change it to a specific state that contradicts what the local controller wants???
|
Follow us on