9/4/2022 4:07 AM | |
Joined: 9/22/2021 Last visit: 8/19/2023 Posts: 1 Rating: (0) |
I have a similar problem, but in my case the two CPU S7 300 2 DP stations are connected via profibus. My CP is connected via profibus as well and I do see where my fault comes in. Could someone help urgently? PR ------------------------------------------------------------------------------------------ AttachmentCHALLENGES NETPRO CONFIGURATION.pdf (477 Downloads) |
Last edited by: The Helping Hand at: 09/05/2022 12:38:40New subject after splitting |
|
Follow us on