10/27/2022 3:34 PM | |
Joined: 7/11/2022 Last visit: 2/15/2023 Posts: 18 Rating: (0) |
Hi everyone, I have a little problem. I am currently learning Tia Portal. If I want to write a program and want to load the program into the virtual plc, currently I can only do it through PLCSIM Advanced and select PLSCIM Virtual Ethernet Adapter in the PG/PC interface of the Download to device page. If other methods are selected in the PG/PC interface, the program cannot be loaded into the virtual plc. The error message is shown in Figure 1. I would like to ask, how can I set the PG/PC interface if I want to load the program into a virtual plc or even a real plc by other ways? For example, as shown in Figure 2, I want to choose Realtek PCle Gbe Family Controller as PG/PC interface Thx for your answer. AttachmentFigure.zip (120 Downloads) |
Follow us on