12/22/2022 9:41 AM | |
Joined: 12/9/2022 Last visit: 4/12/2024 Posts: 7 Rating: (0) |
Hello all, we have a problem since we started the OPC client and collect 5 Boolsche variabels from the PLC. If we start the client we have problems with the HMI reactiontime, sometimes we need to wait 5 seconds till we can press some Button on the HMI. When we stopp the client this issue is directly away. We use the CPU 1515TF-2 PN = 6ES7 515-2UM01-0AB0 Attached some information about the cycletime, connectionressources and Session diagnose. Can someone explain where the problem is and how we can fix it? If you need more information, please tell me what you need. Thanks a lot! Yannik AttachmentInformatione_PLC.pdf (120 Downloads) |
12/22/2022 1:55 PM | |
Joined: 12/9/2022 Last visit: 4/12/2024 Posts: 7 Rating: (0) |
only 15%. |
Follow us on