1/16/2023 10:14 AM | |
Joined: 12/22/2022 Last visit: 5/22/2024 Posts: 10 Rating:
|
Hi Team support, If you refer attachment and follow it the sending SMS all points i.e. any network partner mentioned is achieved but receiving only one SMS is achieved. On Pg#7 following points of receiving many SMS is not achieved which is Pt#1 and from Pt#2 to Pt#5 are followed but only one SMS from one network partner is achieved. The point is as follows: 1. Restrict the partner phone number in the RCV program block [DB3] under "connect.PhoneNumber". The entry "*" means that any number is authorized to send an SMS message to the CP. Similarly on Pg#8 of attachment under Authorizing the phone numbers in a new station Pt#2 is again not achieved which is as follows 2. Enter "*" to accept all phone numbers or enter the relevant number. This function corresponds to the "connect.PhoneNumber" parameter on the TRCV_C block described above. In both the cases achievement is same i.e. to receive SMS from many number or which are mentioned in security for maximum 10 authorized numbers but only one SMS for 1 authorized number in security is achieved. I request support team to guide further exactly what is missing. Attachment109808310_NET_Send_Receive_SMS_Project_DOC_en.pdf (92 Downloads) |
Last edited by: Aumkar at: 01/16/2023 10:15:18 |
|
Follow us on