3/7/2023 6:50 PM | |
Joined: 3/11/2007 Last visit: 5/21/2024 Posts: 226 Rating: (13) |
I have to acquire data from some sensors connected to a control unit that communicates in profinet. I have imported the GSDML file into the TIA Portal. I can establish the connection between PLC (CPU 1214) and the control unit in profinet. It's not very clear to me how to read the sensor data. According to the manual, which I attach link, the sensors are identified with an ID number The GSDML file has configured a read-only data exchange of 15 Bytes. The first Byte of the exchange area, according to the manual contains the sensor ID. What is not clear to me, how to recall the sensor (ID) of my interest since the 15 bytes are read only. Could you help me understand? Thank you Link manual: https://www.ysi.com/File%20Library/Documents/Manuals/ba76148-IQSN-FieldBus-YSI.pdf Attachmentba76148-IQSN-FieldBus-YSI.pdf (97 Downloads) |
Last edited by: automatizzando at: 03/07/2023 18:51:31Last edited by: Jen_Moderator at: 03/08/2023 08:05:24Manual attached from link. |
|
Follow us on