3/24/2023 2:35 PM | |
Joined: 1/21/2013 Last visit: 8/4/2024 Posts: 3044 Rating:
|
Hi Ravi_Mechatronics, Unfortunately, I don't know what SIEMENS_TSEND is and I can't find any information about it. So I can't answer without more information. However, the name indicates a relationship to the so-called T-blocks, which are used for open user communication. For writing parameters to a PROFIBUS slave, however, WR_REC is usually used. Kind regards |
3/24/2023 5:24 PM | |
Joined: 7/22/2022 Last visit: 3/28/2024 Posts: 42 Rating:
|
Using WR_Rec at a time only 39 parameter can be written . I am tying a find a way to transfer attached DB with 55 parameters data in single shot or bulk move or some other way at a single time to profibus slave . If you have any other options , plz suggest me Thanks in advance
|
Follow us on