3/31/2023 9:52 AM | |
Joined: 7/19/2022 Last visit: 10/18/2024 Posts: 403 Rating: (65) |
Hello RamboPLC, I believe that to do the data exchange between the two CPUs it should be done by ethernet based protocol. Therefore, you should have one CP 343-1 for the S7-300 and then do it as indicated in the following FAQ: |
Last edited by: JBS98 at: 03/31/2023 09:53:00If this Information really helps, you could use the Rate function |
|
Follow us on