6/3/2009 8:35 AM | |
Joined: 3/21/2006 Last visit: 4/25/2024 Posts: 10228 Rating: (1181) |
Hello, Look at http://support.automation.siemens.com/WW/view/en/11870489 (Fig. 05) about necessaries settings in PG. In your case instead CP5512(MPI), you'll have PC (MPI). regards Hristo Mihalev |
Last edited by: O_Moderator at: 9/16/2010 2:44 PMlink edited |
|
6/3/2009 8:43 AM | |
Posts: 20 Rating: (0) |
Yes, I am using CP5512 card in PCMCIA slot of my laptop. address set to 0. |
6/3/2009 9:16 AM | |
Posts: 691 Rating: (36) |
You can try one thhing Select CP5512(Auto) in the Set PG/PC Interface and the Click on "Properties -> Start Network Detection It will show the Network Settings i.e Baud rate , Address also and also try it by changing the local address AttachmentSet PG PC.zip (61 Downloads) |
Follow us on