9/14/2023 7:32 AM | |
Joined: 9/21/2022 Last visit: 1/8/2024 Posts: 5 Rating: (0) |
Hey, I have similar problem, Can you explain how did you solve the problem. I am trying to establish OPC UA connection. I use CPU 1212C DC/DC/Rly with external Connection to server, I use an unmanaged switch for the filed device and the external ethernet connection is also connected to the same switch. I can ping PLC in local network but not through remote network.
------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 09/14/2023 10:45:07New subject after splitting |
|
9/18/2023 12:05 PM | |
Joined: 6/19/2017 Last visit: 9/6/2024 Posts: 8175 Rating: (172) |
Closed cause question posted twice. The second thread with the subject Ethernet cable connection Between PLC and OPC is published within the conference Communication / Networks. Jen_Moderator |
Follow us on