2/19/2024 12:16 PM | |
Joined: 7/9/2015 Last visit: 11/18/2024 Posts: 4028 Rating: (603)
|
Hi, I can´t believe, that there is no error / status available. Do you check error and save status? Do like described here: How do you evaluate the status of system blocks in STEP 7 (TIA Portal)? |
|
|
2/19/2024 1:51 PM | |
Joined: 2/19/2024 Last visit: 6/18/2024 Posts: 3 Rating: (0) |
Dear Sir, Thanks for your reply. I have checked the error code before establishing connection and after initiating connection but it stays constant 16#7000. I have attached Photo for the same. Kindly check. Error code stays constant 16#7000 before and after initiating communication. No change. My CPU firmware Version is 2.8. Does that causing this issue ? AttachmentTCON.zip (375 Downloads) |
2/19/2024 4:47 PM | |
Joined: 3/30/2020 Last visit: 11/18/2024 Posts: 4967 Rating: (1012) |
Sorry if I created the illusion that I have all the knowledge you need. I am not familiar with Hitachi. The specification sheet did lead to the clues. You can review the application example for the S7-1500 side: How do you program and parameterize Modbus/TCP communication between S7-1500 CPUs and S7-1200 CPUs? The first step you should make is to decide which side gives the information (server) and which side takes the information (client). On the server side you need to configure which memory locations are made available to the client. The client is normally the partner that establishes the connection. You can either hold the connection or make connection only for the while a transaction is being processed. It is possible for the S7-1500 to be server and client. The only restriction is that a new resource with another port number needs to be configured. You will need to find out from people who know the Hitachi on what is expected on that side. Good luck with your project. |
Activities of this user is voluntary. There is no obligation or liability placed on this user. Though optional, your 'please' and 'thank you' is highly valued. |
|
Follow us on