6/21/2024 8:38 AM | |
Joined: 5/29/2024 Last visit: 6/26/2024 Posts: 11 Rating:
|
Hi AutoGen_7073121! I explain the differences between "Minimum publishing interval" and “Minimum sampling interval”: -> "Minimum publishing interval": This value determines at what minimal intervals the OPC UA server is allowed to send data to a client via OPC UA subscriptions. -> “Minimum sampling interval”: This value determines at what minimum intervals the OPC UA server is allowed to request data changes of the CPU data management. The minimum value depends on the CPU type. In this link you can find more information about OPC UA client communication: https://support.industry.siemens.com/cs/ww/en/view/109737901 If this Information really helps, you could use the Rate function Best Regards, |
If this Information really helps, you could use the Rate function |
|
6/25/2024 12:58 PM | |
Joined: 8/3/2009 Last visit: 6/26/2024 Posts: 13140 Rating:
|
Hello there are also a few iniformation avilable about performance of the OPC UA Server/PLC: https://support.industry.siemens.com/cs/de/en/view/109766727 Bye Murof |
If this Information really helps, you could use the Rate function |
|
Follow us on