2/5/2024 12:50 PM | |
Joined: 5/18/2015 Last visit: 5/8/2024 Posts: 98 Rating: (1) |
Hello i have similar problem when i want write NC Archive on controller , i see '' memory is full'' i do '' NC general RESET '' To bring the control system into a defined initial state, initialization (NC general RESET) is required when the power is first connected. To execute an NCK RESET, place turn start-up switch S3 on the NCU to position 1 and switch on the control. The control then boots, the SRAM memory is erased and the machine data are preset to the default values. and ''Booting via HMMI/MMC'' NC booting can also be initiated via the soft key “NC RESET” in the Diagnostics operating area (corresponds to position 0 on start-up switch S3). The message “Start-up successful” appears in the status line. but i can't still write NC Archive. is there other way ?? ------------------------------------------------------------------------------------------ AttachmentSINUMERIK 840D Memory is full.pdf (479 Downloads) |
Last edited by: Jen_Moderator at: 02/06/2024 07:27:59New subject after splitting SKAZEMCNC |
|
Follow us on