8/14/2024 7:34 AM | |
Joined: 5/22/2012 Last visit: 11/8/2024 Posts: 8 Rating: (0) |
Hello, how can a faceplate that was opened as a popup get the "popupWindowName" of it selve? ------------------------------------------------------------------------------------------ |
Last edited by: Moderator_Lan at: 08/14/2024 08:42:24New subject after splitting |
|
8/15/2024 9:39 AM | |
Joined: 8/3/2009 Last visit: 11/15/2024 Posts: 14176 Rating: (1774)
|
Hello Daniel L. PLP There is a good example how to search: https://support.industry.siemens.com/cs/ww/en/view/109810540 Bye Murof |
If this Information really helps, you could use the Rate function |
|
8/16/2024 8:30 AM | |
Joined: 5/22/2012 Last visit: 11/8/2024 Posts: 8 Rating: (0) |
The Problem is in the opened Faceplate i dont have the name of the popup Window |
8/28/2024 7:35 PM | |
Joined: 1/21/2013 Last visit: 11/15/2024 Posts: 3277 Rating: (509)
|
Hi Daniel, Starting with V18 Update 3, the OpenFaceplateInPopup method has some additional parameters. One of them is popupWindowName, which specifies the name of the popup window. See the readme for details. These changes are not mentioned in the V18 and V19 manual because the update was released later. Kind regards |
This contribution was helpful to1 thankful Users |
Follow us on