9/16/2024 11:35 AM | |
Joined: 2/26/2024 Last visit: 11/14/2024 Posts: 65 Rating: (0) |
Would you be able to provide an example? Thanks. |
9/20/2024 12:17 PM | |
Joined: 2/26/2024 Last visit: 11/14/2024 Posts: 65 Rating: (0) |
Interested. Can you provide the example. Thanks. |
9/20/2024 12:33 PM | |
Joined: 2/25/2016 Last visit: 10/17/2024 Posts: 13 Rating: (7) |
There are a couple of parameters that probably need clarification. Speed I set the value from 0 to 100. At 100 it will move as fast as possible, at zero it will not move. LineWidth and DashWidth sets the line width and thickness in pixels. Run starts the animation.
Attachmentdashes_svghmi.zip (170 Downloads) |
Follow us on