(0)| 7/31/2025 12:49 PM | |
|
Joined: 7/22/2025 Last visit: 12/25/2025 Posts: 40 Rating:
|
can i read other parameters from drive like motor current, power and voltage? ------------------------------------------------------------------------------------------ |
Last edited by: Moderator_Lan at: 07/31/2025 13:09:18New subject after splitting |
|
| 7/31/2025 1:35 PM | |
|
Joined: 7/31/2020 Last visit: 12/19/2025 Posts: 426 Rating:
|
Hello, Can you tell us which drive and which software you want to read from? Best regards |
| 7/31/2025 8:34 PM | |
|
Joined: 7/7/2010 Last visit: 12/23/2025 Posts: 16325 Rating:
|
If you are using Sinamics Starter to commission the VFD(s), you can easily modify the telegram. However, in the interest of saving you a lot of headache, I recommend configuring your VFD first with telegram 352. Once that is done and the PLC and VFD are communicating correctly, modify the telegram in the VFD using Starter to Free Telegram 12/12. Then you can modify the newly added telegram words (leaving the existing and working Telegram 352 parameters alone) to whatever parameters you wish. Keep in mind, Telegram 352 will give you motor current and torque built into that telegram, so you would only need to add power and voltage. Keep in mind you also need to set the proper 100% reference values in the VFD (p200n's) and use those to rescale the -27648 to +27648 data coming from the VFD for current, torque, power, and voltage. There are many forum posts and online FAQs and manuals discussing this at length.
|
|
science guy |
|
| 8/4/2025 9:35 AM | |
|
Joined: 7/22/2025 Last visit: 12/25/2025 Posts: 40 Rating:
|
TIA V19 and PLC1500 with GSD of G120X drive running 3ph motor, telegram specified in drive is by default telegram 1 |
Follow us on